MX0020A/21A/22A/24A/25A Probe Amplifiers

Sample of the MX0020A, MX0021A, MX0022A, MX0024A, and MX0025A InfiniiMax Ultra Series Probe Amplifiers.The InfiniiMax Ultra probing system is the most recent generation of InfiniiMax probing system with:

The InfiniiMax Ultra probe amplifiers address modern high-speed probing requirements by offering up to 25 GHz bandwidth and RC input impedance profile for extremely low midband loading . It provides a wide variety of flexible connectivity solutions, covering today’s emerging signaling standards such as DDR5/LPDDR5 and other high-speed signal debug and validation test needs.

This probe amplifier is compatible with the Infiniium AutoProbe ll Interface which completely configures the Infiniium series of oscilloscopes for this probe amplifier.

This probe amplifier has built-in probe specific s-parameter correction filter to ensure a flat frequency response. This unique s-parameter of the probe amplifier is used with the s-parameters of various supported probe heads to further flatten the magnitude and phase response of the probe for high accuracy measurements.

InfiniiMax Ultra Series Family Diagram

As illustrated in the following picture, the InfiniiMax Ultra probe amplifiers support the new higher bandwidth InfiniiMax Ultra probe heads as well as the existing InfiniiMax I and II probe heads listed in this picture.

Note: Only the recommended probe head configurations for InfiniiMax Ultra series probe amplifiers are listed in this diagram. This is not a comprehensive list of all compatible probe heads. For a complete list of compatible probe heads for these amplifiers, please see the data sheet or the compatibility table provided for each probe head in this Probe Resource Center.

Click on items in this picture!

InfiniiMax Ultra series family diagram showing compatibility between supported oscilloscopes, InfiniiMax Ultra probe amplifiers, adapters and accessories, and recommended InfiniiMax Ultra, InfiniiMax II, and InfiniiMax I probe heads and probe tips. Redirects to the page for MX0105A InfiniiMax Ultra Differential SMA Probe HeadRedirects to the page for MX0106A InfiniiMax Ultra Differential Solder-in Probe HeadRedirects to the document for N2852A AutoProbe II to AutoProbe III Interface Adapter User's GuideRedirects to the page for UXR-Series Compatible ProbesRedirects to the page for UXR-Series Compatible ProbesRedirects to the page for MX0100A InfiniiMax Micro Probe HeadRedirects to the page for N2839A InfiniiMax Diff. Browser Probe HeadRedirects to the page for N5381B InfiniiMax Differential Solder-In Probe HeadRedirects to the page for N2851A InfiniiMax II QuickTip Probe HeadRedirects to the page for E2677A/B InfiniiMax Solder-In Differential Probe HeadRedirects to the page for E2678B InfiniiMax Socketed Differential Probe HeadRedirects to the page for E2675B InfiniiMax Differential Browser Probe HeadRedirects to the page for N5425A/B 12GHz InfiniiMax Differential ZIF Probe HeadRedirects to the page for MX0020A/21A/22A/24A/25A InfiniiMax Ultra Series Probe AmplifiersRedirects to the document for N5450B InfiniiMax Extreme Temperature Extension Cable Data SheetRedirects to the page for N2880A In-Line Attenuator KitRedirects to the page for N2881A DC Blocking CapacitorsRedirects to the page for V-Series Compatible ProbesRedirects to the page for N5425A/B 12GHz InfiniiMax Differential ZIF Probe HeadRedirects to the page for E2679B InfiniiMax Solder-In Single-Ended Probe HeadRedirects to the page for E2676B InfiniiMax Single-Ended Browser Probe HeadRedirects to the page for E2679B InfiniiMax Solder-In Single-Ended Probe HeadRedirects to the page for MX0105A InfiniiMax Ultra Differential SMA Probe Head